Load Offline Data Log
While not connected to an instrument, you can load a previously-saved Data Log file and view it in the Offline Data Log Viewer (see below).
Click
, then select "Open Data Log File".
The data log files are stored with an *.ivif file extension in the "Documents" folder on your computer.
For example – C:\Users\<user_name>\Documents\Keysight\PathWaveOscilloscope\Data Logs\.
For example – C:\Users\<user_name>\Documents\Keysight\PathWaveOscilloscope\Data Logs\.
Offline Data Log Viewer
Below is an example of a Data Log file from the Trace Data view loaded in Offline Data Log Viewer.
| 1 | Configure the traces display and data logging settings. See Trace Data Settings Panel. | |
| 2 | View the captured trace data or measurement information from the current data log. | |
| 3 | For Get Current Trace mode, show or hide the "Setup Text" panel at right. See Setup Text. | |
| 4 | Use Trace Display Toolbar to zoom in/out, and auto scale the displayed data. | |
| 5 | Select the chart type. See Data Display Views. | |
| 6 | Export a data log from the application to Microsoft Excel (.xlsx) format or CSV (comma-separated values) format. See Export Data Log. |
|
| 7 | For Get Current Trace mode, show the oscilloscope's setup information. See Setup Text. | |
| 8 | Show portion of data currently displayed on chart above. See Data Preview Bar. |